User Activity

Hi all,Dear all ST's expert, somebody help me out, Thank you very much.An errors occurred while compiling, see below:assembler code:build result:​IDE: SPC5 Studio, version: 5.8.1Compiler: FreeGCC with VLE support or Hightec Pro
Hi all,​Could you check this problem for me? It can not received information from canoe, data(from transceiver) already reached RX pin of SPC5.​The data transmit from Conoe is : ​The source code in Attachment.​I use external OSC is 8M.CanBitRate is 5...
Hi, ST expertsI added component 'SPC5 FreeRTOS Component RLA' to the applicaion of ‘SPC560BCxx_RLA DSPI Test Application’.Found that MCU can not run, the attachment is the source code, experts help to see, what is the problem?I tried to solve this p...
Hi, The program has been in irqSysHalt at the time of clock initialization, the clock initialization failed, but I don't know why? Has anyone encountered a similar problem?Program clock init fail:​The figure below is the clock configuration:​
Hello all,When I call this function osalThreadDelayMicroseconds(1u), I found that 1us is not implemented, and the actual result is 1ms.But if you call osalThreadDelayMicroseconds (9000u) it can reach 9ms.The parameter usec is less than 1000 and is 1m...
Kudos from