Microcontrollers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

[Solved]DPSI MOSI problem

Posted on February 10, 2015 at 08:33when I use DSPI , I send two frames 16bits per frame, and I monitor that there is a pulse inter frame on MOSI pin (suppose I send two frames  0x00000000 ), it is very strange , I checked step and step,when I set M...

270284440 by Associate III
  • 253 Views
  • 4 replies
  • 0 kudos

Resolved! Problem With Virtual Timer

Posted on February 09, 2015 at 07:45Hi I Want to use a virtual timer in my program , i think the code is ok but when i debug it the program all is in this function : static void tmrfunc(void *p) please see the code and say to me what wrong in my p...

How Can write My own Bootlader Program in Spc560b50L5

Posted on February 04, 2015 at 12:17Hi I want to Write My Own BootLoader on SPC560 but for going to boot mode i have Some Probelms : 1.for going to boot mode in this document (32-bit MCU family built on the embedded Power Architecture)  said we sho...

SPC5STudio 3.4.0 is available !

Posted on January 26, 2015 at 16:57SPC5STudio 3.4.0 is available !Dear Users,The 3.4.0 release is now available on the update site.Here are is the change logSPC5STUDIO CORE :- Patch mode: newly created project is already patched- Implementing invisi...

How to use C++?

Posted on February 03, 2015 at 08:57 Hello, I'm trying use Class but not working... Console out: source/PIDControl.h:11:1: error: unknown type name 'class' source/PIDControl.h:11:19: error: expected '=' , ',' , ';' , ...

Resolved! Continous data transfer to GPIO with DMA SPC56EL

Posted on February 03, 2015 at 16:11 Hello, I would like to use DMA to control the states of some GPIOs. The software should write the entries of an array to the PGPDO[0]register. For that case, I wrote a small demo program. The outputAr...

Patriks by Senior
  • 281 Views
  • 1 replies
  • 0 kudos

Including a file

Posted on January 20, 2015 at 14:56Hello,I am using SPC5Studio v3.3.1 and I want to add a C module and a header to the project created by SPC5Studio wizard. I tried adding the same to 'source' folder. I also modified the project properties to includ...

ssk by Associate II
  • 345 Views
  • 6 replies
  • 0 kudos

Start using SPC

Posted on January 23, 2015 at 14:21Hello All,I am new user for SPC series MCU and SPC5Studio as well. I am trying to start with few example codes to understand the HAL, PAL implementations. I am trying to go through different posts on this forum to ...

ssk by Associate II
  • 349 Views
  • 3 replies
  • 0 kudos

Resolved! FlexPWM SPC56EL Driver

Posted on January 16, 2015 at 10:09 Hello, I have some problems using the PWM sample project together with the SPC56xL Discovery board. The project generates different PWM signals on the PWMA pin of submodule0. I was able to adapt the PW...

Patriks by Senior
  • 427 Views
  • 7 replies
  • 0 kudos