Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue  in each corporate company. “"Path building" refers to the pro...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Facing issue with LINFLEX_0: Help needed

Posted on April 23, 2015 at 17:36Hi,I am writing a LINFLEX_0 driver for SPC560B60L3. DMA is not used as of now. All interrupts are disabled.Linflex_0 can be configured in 2 sets of port pins set 1: LIN0TX in PB[0] and LIN0RX in PB[1]. Alternate func...

saswatkd by Associate II
  • 597 Views
  • 3 replies
  • 0 kudos

Resolved! [solved] Interrupt priorities

Posted on November 25, 2014 at 13:18Hello, Yesterday, I investigated a problem with my software project for an SPC560B. There are several calculations running on the controller and it additionally communicates over UART with a PC. When I tried to in...

Patriks by Senior
  • 1519 Views
  • 16 replies
  • 0 kudos

SPC5Studio Login information

Posted on April 15, 2015 at 08:00I am using SPC5Studio with SPC560D MCU for a long time. From couple of days back, when I start the SPC5Studio application it asks for the login information (user name and password) for three different urls. Please fi...

ssk by Associate II
  • 810 Views
  • 5 replies
  • 0 kudos

ADC0 interrupt problem

Posted on April 15, 2015 at 12:14 Hi I Want to use , End of Conversion interrupt in ADC0 but when i set the NSTART bit in ADC0- MCR register in debug mode i saw in SFR view ,ADC0_ISR EOC bit is set but the interrupt is not work. when i use whil...

Warning-Unknown break cause !!!

Posted on April 17, 2015 at 10:55Hello,I am trying to execute a simple serial driver application on my target board. It uses SPC560D30L3 MCU. I have tested the same code using SPC Discovery kit (SPC560D30L3) mounted on it. The code executes successf...

ssk by Associate II
  • 545 Views
  • 2 replies
  • 0 kudos

SPC560Dxx FlexCAN Transmit error

Posted on April 09, 2015 at 12:22I am using SPC560D-DIS Discovery board for development and SPC5 studio.I have imported test application 'SPC560Dxx OS-Less CAN Test Application for Discovery' for FlexCAN testing. In this FlexCAN0 is used in loop bac...

megha2 by Associate
  • 601 Views
  • 3 replies
  • 0 kudos

unable to debug using SPC5-UDESTK

Posted on April 08, 2015 at 09:33Hi there,I am trying to run a test application (SPC560Bxx OS-Less test application) on SPC560B60L5 mounted in SPC560BADAPT144S evaluation board, using SPC5-UDESTK.After generating and building the test application I ...

gilad2 by Associate II
  • 551 Views
  • 3 replies
  • 0 kudos

Purchase of SPC560 MCU

Posted on April 06, 2015 at 12:56Hello Members,I am trying to purchase 10 SPC560D40L3 MCU for building my product prototype. I tried placing the order with ST. I was directed to ST vendor. Even after accepting a lead time of 24 weeks, I am unable to...

ssk by Associate II
  • 361 Views
  • 2 replies
  • 0 kudos

Resolved! Bug in Pinmap Wizard for ADC Use

Posted on April 05, 2015 at 15:54Hi I Want to use ADC of My SPC560B-DIS , first there is not an example for this Dev Board in SPC-Studio but when i want use the other samples for ADC when i want to set ADC pin, in pinmap wizard i have a Warning and ...

codesourcery for PowerPC

Posted on April 06, 2015 at 10:21Hello EveryBody,I'm try to build a project using  the compiler : codesourcery for PowerPC. is their any  tutorial or guidline to help .to use   codesourcery  witch eclipse to compile a project for SPC56 MCU ???