Posted on February 24, 2016 at 13:12Hello,I'm trying my old Flash Library.(for SPC560B50L5) But not working. How is use DFLASH for SPC564B70L7? (debug stop => ''_unhandled_exception:'')Thanks a lot. #dflash
Posted on February 01, 2016 at 14:14Hello,How is voltage regulator requirements for SPC564B70L7?(or regulator circuit) I'm trying but not generated 1.2V core voltage.Thanks.
Posted on February 03, 2015 at 08:57
Hello,
I'm trying use
Class but not working...
Console out:
source/PIDControl.h:11:1: error: unknown type name
'class'
source/PIDControl.h:11:19: error: expected
'='
,
','
,
';'
, ...
Posted on December 17, 2014 at 15:26
Hello,
I'm using SPC5-Studio v3 with 1-year license. I'm recovery my PC. But my old license file not working.
What should I do?
@Edit: licence start date : 2014 , 14:03
@edit console o...
Posted on December 01, 2014 at 12:38
Hello,
I trying use the I2C periph. But, It is not work. Have you a I2C referance manual ? or What should I do?
My Example code :
void
I2C_initial(
void
)
{
/*
* Note: Clk is startup enable...
Posted on February 24, 2016 at 15:31 Hello Erwan, Do you have open source example flash control driver? Other library very complex and not support easy word write and read. Thanks. for Example: /**
* @brief Initializes the drive...