Automotive MCUs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! BSDL file for SPC560B54L3C6E0X

I need the BSDL file (Boundary Scan Description Language ) for SPC560B54L3C6E0X device, but I cannot find it on your web site. Can you send to me?NOTE: This question and answer originated from a customer support case which was handled by us. We regul...

SPC58NN HSM information

Hi,Can someone elaborate on  the Key update programming process for SPC58NN84 controller or any document which can provide this information.

sonal by Associate
  • 285 Views
  • 0 replies
  • 0 kudos

SPC572 with SARADC in DMA mode

We have the SARADC up and running in DMA mode on 1 channel as per the sample application.But when we add 2 more channels we can't get it to go throgh the callback routin. (saradcconfdma_ch1_conf_cb & saradcconfdma_ch2_conf_cb) and hence we don´t get ...

Larsa by Associate II
  • 643 Views
  • 0 replies
  • 0 kudos

SARADC errors after SPC5 uppgrade

Worked perfect 2 years ago, then after updating the SPC5Studio we can´t get the SARADC to compile without alot of errors in the saradc_lld_cfg.c file (attached picture). We tried to use the old saradc_lld_cfg.c file and we could compile it but the ad...

Larsa by Associate II
  • 714 Views
  • 1 replies
  • 0 kudos

Error encountered while building the code

./components/spc574sxx_low_level_drivers_component_rla/lib/include/spi_lld.h:690:2: error: #error "SPI driver activated but no DSPI peripheral assigned"#error "SPI driver activated but no DSPI peripheral assigned" This is the error i encountered whil...

SPC5 GTM Cluster Clock issues

Using the SPC572Lxx RLA GTM DPLL Test Application for Discovery all works fine until for some reason the Cluster Clocks in the Clock Manager Unit of the GTM IP Configuration changes to what´s shown in the picture and we get the Error "2' is not a val...

Larsa by Associate II
  • 477 Views
  • 0 replies
  • 0 kudos

FDA903D unable to play audio out on custom hardware

Hello All, We have designed our own custom hardware using SPC582bxx automotive controller and FDA903D audio amplifier. We built the code test the audio amplifier, code is very simple to play audio. We have used SPC582Bxx Engine simulator code and mod...

Resolved! SPC58EC80 CanBus RTR Frame Request

I'm using SPC58 DISP Board for RTR request data frame from a battery pack. I have set the RTR value as 1, but didn't receive any reponse data frame from the battery. I have tested with CAN analyser, reponse data frame is coming(working fine). When I ...

Screenshot 2024-06-19 185331.png