Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

How to configure ICU eMIOS0 Channel 22 SPC582B60E1MH00Y?

Hi,Im new to SPC582 my issue is I need to enable ICU at eMIOS0 Channel 22 , I have enabled the pin in the pin map editor and in the GUI there is channel enabling option for only CH 0 to CH 7 as SAIC but I want it for CH 22, Is there any way to enable...

Screenshot 2025-08-07 175333.png Rajesh3_0-1754569651526.png
Rajesh3 by Associate
  • 1313 Views
  • 0 replies
  • 0 kudos

SPC58EC-disp EMIOS setup into DAOC mode

Dear,I am trying to setup a channel of the EMIOS into DAOC mode. I walked through an example of using PWM, but I am confused on why in the EMIOS setup i can only set the channels to SAIC (ICU) or OPWFMB (PWM). I tried to manually set the MODE bitfiel...

JTAG Error SPC584b tap ver missmatch

I'm currently try to work with the SPC584B70E1.Debugging with the AEK-MCU-SPC5LNK with openOCD, it throws following error during debugging-initialization:Info : JTAG tap: spc584b.tap tap/device found: 0x20144041 (mfg: 0x020 (STMicroelectronics), part...

ADC with CTU on SPC560P50L

I am currently working on configuring the ADC using the CTU module. However, I’m facing some issues. Can anyone please guide me on how to configure the ADC with CTU, or share some sample code? I'm using the SPC560P50L board with the SPC5Studio IDE.

How to use CAN protocol in bootloader on SPC584Bxx

We are currently conducting CAN communication using the SPC584Bxx chip. We are trying to develop a FW update function using this communication.Are there any guides or related materials for updating the SPC584Bxx chip? If so, please share them with us...