Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Selecting ST ToF Modules for Distance Measurement During Free Fall

Hello community, I am working on a project that involves measuring a precise distance of 2 meters from the ground during an object’s free fall. I am considering using Time-of-Flight (ToF) modules from ST for this purpose and would like some guidance ...

Vect by Associate
  • 1398 Views
  • 1 replies
  • 1 kudos

Resolved! VL6180X laser compliance documents

Hello,We are using the VL6180X in a IVD product and need laser test certificate documents to show the range sensor is class 1 and safe for the user. Can you send me a test reports for this part? I see a CDRH report posted for VL53L1, but couldn't fin...

AJB721 by Associate
  • 1357 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L8 - programmable ROI

Hii ,Does VL53L8 tof sensor support ROI selection or Reduced FoV as VL53L1 , if yes how do i do it ?Thanks,Poornima B

Poornima by Associate
  • 1329 Views
  • 1 replies
  • 0 kudos

VL53L7CX range fluctuation

Hi I am developing a commercial footfall counter based on the VL53L7CX and ESP32.The API is (Version : VL53L7CX_1.2.10)I have produced a mockup using the VL53L7CX breakout board.IOVCC is 3.3 voltsI am using the on board regulator for AVDD powered fro...

RickHamilton_0-1710942131024.png

VL53L4CD - Signal is below the defined threshold

Hey,I have a custom made board/device which is using 4x VL53L4CD Tof Sensors to measure the distance. I have trouble to calibrate the sensors correctly or get correct values from them from time to time. Sometimes it works well - sometimes it does not...

DrD00m by Associate III
  • 11443 Views
  • 27 replies
  • 0 kudos

VL53L3CX measurement never ready

I've been trying to get my VL53L3CX to communicate with my ESP32-S3. I'm using esp-idf and ported https://github.com/stm32duino/VL53L3CX by rewriting the I2C and GPIO code for esp-idf. As far as I can tell, I'm successfully communicating with the VL5...

k1ra by Associate
  • 1590 Views
  • 0 replies
  • 0 kudos

Resolved! VL6180 EOL, VL53 as subtitute

Hello,We received an EOL status notification for our current sensor VL6180 and I found the VL53L4CD as a substitute for this TOF proximity sensor. We would like to know how long this device will be active, as the VL6180 is now on EOL.Can you also con...

finding short library on vl53lox

I am looking for the shortest library for the vl53lox. I am using the b-l475e-iot01a1 board and i just need some measures on the vl53lox.I look on github but there are just a lot of files so I would like to know if  a less heavy approach exist . Furt...

VL53L8CX GUI Issue

Hi Team, I have P-Nucleo-53L8A1 EVK. This board is connected to PC via micro USB cable. LD1 and LD3 LED's are ON and are red in color. I am trying to use VL53L8CX GUI , but its showing at About window as attached.     'Update ST-Link '  process trie...

Deep_bang_0-1715076685998.png
Deep_bang by Associate II
  • 1251 Views
  • 1 replies
  • 0 kudos