User Activity

I am renewing this conversation because I had added this concern to a conversation with the same subject that was marked as solved. Originally posted by @MBela.3 .I have not received a response. However, it is very important to me not only for my app...
I see that the VL53L5CX sensor has two voltage supply alternatives, both for the digital part (IOVDD) and the analog part (AVDD). I am also observing that starting from version 1.3.3 of the ULD driver, we have a function called vl53l5cx_disable_in...
I am using STM32CubeIDE V 1.9.0, with an Nucleo board with STM32F401, and STLink integrated. Debugger just stopped working. I have spent hours trying to change debugging configurations, upgrading STLink firmware, but nothing. When I press Debug I see...
When filling the struct in my apptypedef struct { uint32_t RangingProfile; uint32_t TimingBudget; /*!< Expressed in milliseconds */ uint32_t Frequency; /*!< Expressed in Hz */ uint32_t EnableAmbient; /*!< En...
After been testing VL53L3CX in my own board based in a STM32F407 micro, I want to test VL53L1CB now. But I am not wiring (satellite board) to a Nucleo board. I have connected it to my own board and trying to reformulate the project with STM32CubeMX. ...
Kudos from