Hi I'm currently using your LPS22DFmodule to measure pressure and I saw in the datasheet that the temperature accuracy is ±1.5 °C (T = 0 to 80°C). My working range is between -15°C and 60°C. C...
Greetings I am trying to utilise the FIFO of the LIS2DW12, in bypass-continuous mode, which requires the latched-interrupt bit (LIR) in CTRL3 register to be set, as stated in the application note AN...
Hello Everyone! I am working on a project Ecompass using controllers STM32F401CBU6 and mems sensor ISM303DAC. can able to read raw values of both accelerometer data and magnetometer data properly an...
Hi everyone. I'm trying to use a NUCLEO-F401RE, a X-NUCLEO-IKS02A1, and a STEVAL-MKI197v1 and the following software: v3.2.0.4544 AlgoBuilder, v1.25.1.11665 Unicleo-GUI, v1.15.0 STM32CubeIDE, v...
Hi, I am using AIS2IH. I can see in terminal window of my computer that registers of data and temperature are zero's. 0 0 0 ... My program use the setup:...
hello, i have few basic Question regarding accelerometer sensor. 1. accelerometer data coming from imu sensor that is 2's compliment data, so should i receive this data in signed integer or unsigne...
I'm having problems to be able to establish the connection between STEVAL STWINBX1 and ST MEMS Studio software, with either of the two available ways (BLE or Serial port). In the first ca...
Hello We use a LIS2DW12 accelerometer to mesure tilt over a temperature range from -25°C to +70°C. We set the full scale to 2g and chose High Performance mode with Low Noise enabled. We want an ac...
Hello everyone I need to have the pspice model of LIS344ALH (i know that this product is not longer available) I try do it with the datasheet but i don't have enought info Can someone help wi...