Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! MPC5606B LINFlex5 raising 'Stuck at Zero Flag' interrupt

Hi I have problem with LINFlex5 calling 'Stuck at Zero Flag' interrupt continuously. Voltage on the pin 29 (GPIO4/E0UC4/CS0_1/LIN5RX/WKUP9) is 3.2V nevertheless. It's 100-pin LQFP version so there no other choise for LIN5RX input (using PADSEL60). I ...

snafu by Associate II
  • 1411 Views
  • 2 replies
  • 0 kudos

Resolved! SPC570S GPIO Setup

HI,I have a question regarding the GPIO setup.I have setup a few pins and outputs from the pin map editor. For all of those pins, the togglefunction work without any issue. However when I try to turn them on or off using the write_pad function or the...

NBula.1 by Associate III
  • 3265 Views
  • 6 replies
  • 0 kudos

SPC584B - Issues with CAN RX

Hi,When I use the low level drivers that comes with SPC5 Studio, I am facing issues with CAN reception.The Rx buffer only updates with the highest priority message. All the messages below that are ignored. I tried with FIFO and Dedicated Buffer setti...

SKara.7 by Associate II
  • 1584 Views
  • 3 replies
  • 0 kudos

ADC DMA configuration with different groups

Hi All, We are using the SPC560P50L3 controller in our project. ADC0 and ADC1 are used to read 16 ADC channels.ADC0 is configured with one group with 6 channels, ADC1 is configured with 2 groups. Group1 - 6channels   Goup2 - 4channels.We need to read...

Resolved! Code does not execute when the ADC was setup in "RTOS example" on SPC560P50L5 which comes with spc5 studio?

MCU - SPC560P50L5First I compile and flash RTOS serial example with no errors. then I run it. No errors were detected. same process was followed to check ADC example. There also no error were found. Then I combined both codes as follows(attached). It...

Harsh1 by Associate II
  • 1436 Views
  • 1 replies
  • 1 kudos

Resolved! MPC56 and SPC56 microcontrollers

I have 2 questions.SPC560P50L5 and SPC563M64L5 microcontrollers from ST with which microcontrollers from NXP are compatible (in terms of functions and pins)?Can the output hex file from the MPC56 and SPC56 microcontrollers be replaced?