Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! MPC56 and SPC56 microcontrollers

I have 2 questions.SPC560P50L5 and SPC563M64L5 microcontrollers from ST with which microcontrollers from NXP are compatible (in terms of functions and pins)?Can the output hex file from the MPC56 and SPC56 microcontrollers be replaced?

Resolved! With any of the optimization levels (-Os size/-O1 general/-O2 speed/-O3 fast) except -O0 none, bootloader is not jumping to the application code.

Hi, I am working on SPC58NG84E7 bootloader. I have BL code(at 0xFC0000) which jumps to the APP location 0xFD0000 after waiting for 10sec after startup and executes the code there. Both codes have optimization NONE(-O0). But when BL optimization chang...

AVM by Associate III
  • 2520 Views
  • 3 replies
  • 0 kudos

Resolved! DMEM Processor local RAM Memory configuration Issue

Micro controller : SPC584BWe tried configuring the DMEM Processor local RAM for SPC584B Microcontroller.(Attaching the DMEM Memory layout) (We have configured it outside BAF region)We tried pushing initialized global variables to this section. We hav...

JJose.4 by Associate
  • 2267 Views
  • 1 replies
  • 0 kudos

How to use ICU for channels in eMOIS0 Group1 with SPC5Studio?

Hi,I am using SPC584B70E3 and I want to configure some of the inputs as an ICU. However, the SPC5Studio Limits the ICU for eMIOS0 Channels 0-7 only. I cannot configure PE[0] (eMIOS0 Channel 11 or eMIOS1 Channel 13) as ICU for instance. In the Referen...

TUyar.1 by Associate
  • 3925 Views
  • 5 replies
  • 0 kudos

UDE Workspace refers to older source files

Hello,I normally copy an old SPC5 project and paste it with an updated version number to modify the source code. But, the copied UDE workspace is referring to older source code. Can you help to fix it?Thanks in advance.Br,Sreejith

SKara.7 by Associate II
  • 1896 Views
  • 4 replies
  • 0 kudos