User Activity

I am a thesis student and part of my thesis is to test the CAN of SPC58NN84x MCU in two modes, the normal mode, and the loopback mode.The loopback mode is ok as the CAN receives the same message that it transmits properly, however, this is not the ca...
I am doing my thesis on Bernina SPC58NN84x and I am trying to implement a CAN bus between the two CAN Subsystems, so that one of them is receiving and the other is sending, but when I do this the CAN TX doesn't recognize the success of the sending an...
I have used the default test bare-metal application for the testing the can in SPC5 studio stopped the loopback, swap the RX ID filters in the configurator, and tried to send using one can subsystem and receive by the  other but it keeps stuck in th...