Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC5x pinout

Hi, where can I find microcontroller pinout?I miss something? I can't find spc5 pinouts in datasheets, where are these resources?​Best regards​

GMG by Associate III
  • 2358 Views
  • 3 replies
  • 0 kudos

Bootloader and application issue with SWT component

Hi,I am working on SPC58NG84E7 bootloader. Everything works fine - I have BL code(at 0xFC0000) which jumps to the APP location 0xFD0000 after waiting for 10sec after startup and executes the code there. Both codes are without SWT.Issue - But when I a...

AVM by Associate III
  • 7375 Views
  • 21 replies
  • 0 kudos

[SPC58Nxx] GTM 344 and TOMs granuliarity?

Hallo Everyone,If I setup two TOM channels with the TOM module clocked at 100MHz: (10nSec)GTM clocked at 100MHzCMD.CFGU.EN_CLK0 = trueCMD.CFGU.CLK_DIV0 = 1TOM0 module enabledTOM0_4 source clock = CMU_FXCLK0TOM0_4 period = 10000TOM0_4 duty = 5000TOM0_...

CoolMo by Associate III
  • 1849 Views
  • 2 replies
  • 0 kudos

Flash Erase for SPC58NG84E7 is not working

Hello,I am working on the bootloader, trying to flash only 256 bytes. So, before flashing, erasing the block 0xFF0000. There is already some data in this block. But erase is not happenin, even if FlashErase() returns 0 and FlashCheckStatus() also giv...

0693W00000JNFt8QAH.png
AVM by Associate III
  • 9941 Views
  • 23 replies
  • 1 kudos

Can pulses greater than 5ns be detected by mcu?

HiCan any Mcu detect a 5ns wide pulse? Is MCU clock speed important in this case? Or are MCU pin speeds important?Are MCUs capable of detecting such a low amplitude signal?Many thanks for any guidance provided...

Burakgvl by Associate II
  • 2187 Views
  • 3 replies
  • 0 kudos

How to send SPI command by "PIT" every milisecond ?

hello everyone;I’m trying to send some SPI command by SPC560 microcontroller. During the main program I must send a special code regularly, for example I must send the code “0xAAAA�? and “0xBBBB�? every 20mS. Actually when the main program is running...

0693W00000JOOljQAH.png
Bgh.1 by Associate II
  • 1164 Views
  • 1 replies
  • 0 kudos

SPC58EC80E5 current limit on 5v and 3.3v pins

Hi there,I was looking for the current limit on the 5v and 3.3v pins of the SPC58E80E5 board (I check in the user manual) but I can't figured out.Which ones are they? Where I can get this information?

RD'Ig by Associate II
  • 2044 Views
  • 3 replies
  • 0 kudos