Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Spc5 Studio

helloI have just started working with SPC5 studio and I want to use PEMicro for debugging, but no matter how much I searched, I couldn't find anything that could help me in this way. My main problem is that I can't I set the software to PEMicro to de...

spc582b code flash erase/write

I Use SPC582B-DIS Board and i use flash driver provided in ST with DOC UM2636(Standard Software Driver for C55 Flash module embedded on SPC58 B, C, E, H, G and N lines microcontroller). My code booted from 0x00fc0000 in low address. and modify the la...

JINY by Associate
  • 1002 Views
  • 0 replies
  • 0 kudos

Brown Out Reset in SPC584B

Hi,I am using SPC584B70E5 and I need to read the Brown Out reset condition in the controller by reading the reset register. I could not find any reference in the controller manuals to do the same.Is it possible to identify the Brown Out condition by ...

Rejitha by Associate II
  • 1289 Views
  • 1 replies
  • 0 kudos

SPC5 Flash Programmer End Of Life support?

Hello SPC5 Community,I'm using SPC5 Flash Programmer since few years to transfer binaries on SPC564B74L7 as it easier for OEM than JTAG and because there is no access to JTAG on some device we created.On my last licence request (to:apgtools-license@s...

SPC58EC with CAN BUS and UART

Hello dear Engineers.I am using SPC58EC Dev. board and want to use CAN BUS and UART in the same time. I can send Enter command from my keyboard to SPC58EC board via USB to TTL module (TX RX pins). But how can i do that, when i press enter it can send...

Nurlan13 by Associate
  • 1064 Views
  • 0 replies
  • 0 kudos

Running code without debugging (SR5E1-EVBE7000P)

Hello,I'm trying out examples for the SR5E1-EVBE7000P development board. I use StellarLINK to implement the code on the flash and when I run it via RESUME the code runs. But if I execute Terminate and want to run the code without StellarLINK, e.g. by...

What does "Enable All Peripherals" in AN3324 mean?

The Application note AN3324 (Implementing power-on self tests for SPC56EL60 in locked step) says in Figure 2 (page 9) that one should "Enable All Peripherals" before initializing the FCCU. What does "enable" mean in this context? Does it mean setting...

DaveJ by Associate II
  • 738 Views
  • 0 replies
  • 0 kudos

spc58 jtag/Nexus

I through Nexus to read/write memory.Is the response correct?The steps to enter Nexus from jtag are as follows:1. TDI: Shift-IR(0x01) Shift-DR(0x00000000) TDO: 0x11140041it confirms the jtag id is correct2. TDI: Shift-IR(0x2A)it through jtag to enabl...

and_w_0-1732692150611.png
and_w by Associate
  • 934 Views
  • 0 replies
  • 0 kudos