User Activity

Hi, I am developing SPC58EG in SPC5 Studio.I want to use I2C communication with a RTC device.However, I cannot find any example for I2C in the IDE.How do I get the reference to develop I2C?Thank you.
I am developing Lin function(UART) for SPC58eg in SPC5Studio.I cannot build the project of the title because the project cannot  be included stdint.h file in SPC5Stusio.However, I can build the Can Test Application and it includes stdint.h.How can I ...
I am currently developing UART functionality on the SPC58EG chip, and I want to use LinFlexD1 hardware channel to develop UART.However, I cannot find relevant examples in the SPC5 Studio IDE.I am referring to the official manual (RM0391), which menti...
The error will appear when I configurate the module of AdcGroupDefinition, but the port and the hardware channel are configuarted correctly and conform. How can i solve this problem from the picture?   category : Errorproject : Cho6M_Gpt_rtm2descript...