Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC58 data sharing between two cores

I've been using for a bit a SPC58 eval-board and i was wondering how to share global variables between the two cores. I searched around on the internet finding nothing useful. Is "volatile int" enough even for a rough and dirty data sharing or should...

Help setting up L9177A

When replacing L917A how should I reboot it, what hardware or software do, I need please help.*This post has been translated from Persan to comply with the ST Community guidelines.

1000060465.jpg
Savin by Associate
  • 1079 Views
  • 0 replies
  • 0 kudos

Issue faced while debugging AEK-AUD-C1D9031

While debugging the board AEK-AUD-C1D9031 , the SPC5-UDESTK is not responding and it says this always even when the target power supply is turned ON and the Device is shown in Device manager. I think there will be some target configuration which I ha...

nanda_kishore_0-1736500409463.png nanda_kishore_1-1736500424939.png

SPC56EL54 - RESET pin is always  pulled down by the CPU

HiOn power up the SPC56EL54L5CBFS looks like it is in an internal RESET mode that does not  end. The RESET pin is always  pulled down by the CPU. Power up of 1.2v and 3.3v in 1.5msec. Can you help to to understand why the RESET pin is always  pulled ...

Boot Test Firmware from SRAM - SPC58NH92C5

I’m engineer from EMS company. For one of our customer we are going to manufacturing PCBA (Vehicle Control Module) based on SPC58NH92C5 uC. Our customer is owner of design and our customer develop the final firmware for product. However for the manuf...

darwoz by Associate
  • 914 Views
  • 0 replies
  • 0 kudos

Stellar SR6G7 OTP Programming

I would like to know some information about OTP programming in production for the Stellar SR6G7. What are the pins required to set the high voltage? I couldn't find clear information about VDD_OTP in the reference manual. According to the reference, ...

mesutozi by Associate
  • 1339 Views
  • 1 replies
  • 0 kudos

Resolved! Spc5 Studio

helloI have just started working with SPC5 studio and I want to use PEMicro for debugging, but no matter how much I searched, I couldn't find anything that could help me in this way. My main problem is that I can't I set the software to PEMicro to de...