Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

MCU SPC58

Hi anyone could help me how to read this ecu infineon micro using bootmode?oR HOW TO READ THIS FLASH MEMORY

image_67511809 (1).JPG image_67239681.JPG
rashed420 by Associate II
  • 3156 Views
  • 3 replies
  • 0 kudos

Resolved! SPC5 Studio

Hello, I am Erdem.I am an R&D engineer at Devimsel Elektronik. I will use the SPC560P processor on my own PCB board. For this I need instructions for using SPC5 studio. How do I make configurations such as pin and clock tree? Can I get an instruction...

Eakso.1 by Associate II
  • 6016 Views
  • 6 replies
  • 1 kudos

Resolved! EV-VN9D30Q100F for SPC582B-DIS or SPC58EC-DIS GUI firmware

Hi,i need some help for the EV-VN9D30Q100F. It says there is a dedicated Software for the SPC582B-DIS or /EV but i can't find it nowhere. The board connects to the GUI (STSW-EV-M09SPI), so far so good, but without the firmware on the MCU, i can't tes...

PNeub.2 by Associate II
  • 1471 Views
  • 1 replies
  • 3 kudos

Resolved! SPC560P50L5 CAN Module doesn't work successfully

Hello everyone.Because I need to test a newly purchased SPC560-DISP, I tested several commonly used modulesAnd these is my test devices:Devices Used:MCU: SPC560P-DISPCAN: Kvaser Leaf LightV2I conducted tests on several commonly used modules:PITEIRQPW...

Louie33 by Associate II
  • 2085 Views
  • 3 replies
  • 2 kudos

Resolved! searching for datasheet SPC58VX829348

i have looked everywhere and cant find the datasheet for this mcu, we get alot of this becouse we are in the business of reusing dismantled ev car batteries and as much components as possible.with this we are building Energy storages for grid service...

sebbeben by Associate
  • 2151 Views
  • 2 replies
  • 2 kudos

SPC58EC80E5- ISOSPI Launching error

Dear all,I am using AEK-POW-BMS63ENA connected via AEK-COM-ISOSPI module to  AEK-MCU-C4MLIT1 for measuring the voltage, current and temperature of 14 lithium ion battery cells connected in series.after running the demo provided in AutoDevKitStudio, (...

error.JPG signal-2024-11-13-223541_002.jpeg

Protocol conversion box about debug over can

I was recently debugging a product based on SPC58EC80 and wanted to use its debug over CAN feature. I'm using the lauterbash debugging tool, but I can't find the conversion box which converts the debug information to the CAN protocol. Where can I buy...

Resolved! ADC example for SPC560B-DIS not working

I imported the SPC560Bxx_RLA ADC example. As I understand, this example use ADC conversion with DMA, and the ADC value will be converted to the delay time between each time LED D8 is toggled.But some type like uint32_t could not be resolved and I tri...

fiinfi by Associate II
  • 2164 Views
  • 2 replies
  • 0 kudos