Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC564B74 FlexCANs are limited to 32 Mailboxes instead of 64

Posted on September 02, 2015 at 15:30Hello, I'm using SPC5Studio V3.6 and SPC564B74. The HAL drivers are limiting FlexCAN mailbox number to 32 but this CPU has 64 MB per FlexCAN. I can change SPC5_CAN_NUM_RX_MAILBOXES and SPC5_CAN_NUM_TX_MAILBOXES d...

Microcontroller Boot

Posted on August 28, 2015 at 17:09Hello,I can't find any application ( sample code exemple ) for Alternate Boot Sectors, and /or  Serial Boot Modefor SPC560. Best regards

Use CAN mask Filter in addition to filter mode

Posted on August 31, 2015 at 15:23Hi all, i am using SPC560D with SPC5 Studio. Is it possible to use CAN masking by activated Filter Mode (FEN disabled) ? I am not using a CAN interrupt service routine, i am polling the Mailboxes cyclic. Thanks in a...

borbe by Associate
  • 767 Views
  • 0 replies
  • 1 kudos

Pinmap wizard import/export between projects?

Posted on August 28, 2015 at 16:07Hello, In SPC5 Studio V3.4.4, instead of accessing the pinmap wizard using the small icon in the HAL configuration, I created a pinmap wizard in the project using ''New -> SPC5 Studio Pinmap Wizard'' and I'm now stu...

Problem With LINFLEX1 Interrupt

Posted on August 25, 2015 at 09:44Hi In my system i set the LINFLEX1 For my Lin Connections I set this in Master Mode i send and recive correctlly the slave response but i don't have any interrupt on Vector99 what is the problem on SPCstudio ?? Tha...

driver flash SPC560B

Posted on August 21, 2015 at 16:27hello work with SPC5 v3 and chibios.i don't find the source code for Standard software driver for C90FL.to operate on the Flash module embedded on a microcontroller (SPC560B)and a exemple to used the driver.Best reg...

SPC56EL60L5CBF Exceptions

Posted on July 06, 2015 at 09:16Hello,I have a few questions regarding exceptions in microcontroller mentioned in the topic. I'm trying to cause Illegal instruction exception (IVOR6) by substituting part of hex with 0x0000. According to PowerISA v2....

dariusz by Associate II
  • 2017 Views
  • 5 replies
  • 0 kudos

SPC5 examples

Posted on August 26, 2015 at 12:09HiI've installed SPC5 studio v 3.5 and I can't find nowhere these examples:http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00098036.pdf?s_searchtype=keywordWhere can I fin...

How Can i Toggle Pin in standby mode ?

Posted on August 09, 2015 at 14:55Hi members I want to toggle pin in standby mode but i do not know how can i do this ? because when i go to standby mode all things i use is disabled , i saw something lik this in freescale MCU's but i do'nt know how...

SPC5Studio configuration

Posted on August 25, 2015 at 08:27Hello,I am using SPC5Studio for SPC560D MCU. 1. How can I access CTU configuration from SPC5Studio?2. How can I configure ADC module for using CTU, one shot conversion vs scan, priorities for EOC etc?3. Any user gui...

ssk by Associate II
  • 1161 Views
  • 4 replies
  • 0 kudos