2015-02-03 7:11 AM
Hello,
I would like to use DMA to control the states of some GPIOs. The software should write the entries of an array to the PGPDO[0]register. For that case, I wrote a small demo program. The outputArray isuint16_t and contains 256 elements.Each element stands for a state of 8 GPIO pins. The software should write these elements circular to the PGPDO[0] register, but it doesn´t work. The configuration looks like that: edmaChannelStart(0);
edmaTCDSetWord0(edmaGetTCD(0),&outputArray);
edmaTCDSetWord1(edmaGetTCD(0),1,1,2);
edmaTCDSetWord2(edmaGetTCD(0),512);
edmaTCDSetWord3(edmaGetTCD(0),-512);
edmaTCDSetWord4(edmaGetTCD(0),&SIUL.PGPDO[0].R);
edmaTCDSetWord5Linked(edmaGetTCD(0),0,0xFF,1);
edmaTCDSetWord6(edmaGetTCD(0),0);
edmaTCDSetWord7Linked(edmaGetTCD(0),0,0xFF,EDMA_TCD_MODE_START);
Can anybody tell me what I have to change in my configuration when I want the DMA transfer to run continuously as fast as possible?
Best regards,
Patrik
Solved! Go to Solution.
2015-02-05 7:06 AM
Hello,
I have found the problem. I think it was a combination of wrong channel config and DMA_MUX config. The following code gives me a continuous transfer of the array elements to the PGPDO port. The DAC2Table contains 128 16bit elemements.
DMAMUX.CHCONFIG[3].R = 0x00;
DMAMUX.CHCONFIG[3].R = 0b10001110;
EDMA.DMAERQL.R = 0xFFFF;
edmaChannelSetup(3,&DAC2Table,&SIUL.PGPDO[0].R,2,0,1,1,2,128,-256,0,EDMA_TCD_MODE_START);
I was also able to trigger the transfer of an array element using PIT and the triggered functionality. Nevertheless, I have again some problems in understanding how to use DMA with other modules.
It is really hard to get detailed information out of the reference manual and I didn´t found any application notes for the SPC56EL regarding this topic.
In DMA_MUX section, I saw the possibility to use the eTimer module as DMA source. Table 173 shows two sources for eTimer_0 - Channel0 and Channel1. But what does this mean? What kind of request connects the eTimer to DMA?Are they regarding to the capture and compare registers? And how do I use the eTimer in combination with DMA?
What I want to do is to trigger the transfer ofan array element when theeTimer produces a compare event. The eTimer should reload the load the new compare value from the compare load register, which should then be updated by DMA.
Best regards,
Patrik
2015-02-05 7:06 AM
Hello,
I have found the problem. I think it was a combination of wrong channel config and DMA_MUX config. The following code gives me a continuous transfer of the array elements to the PGPDO port. The DAC2Table contains 128 16bit elemements.
DMAMUX.CHCONFIG[3].R = 0x00;
DMAMUX.CHCONFIG[3].R = 0b10001110;
EDMA.DMAERQL.R = 0xFFFF;
edmaChannelSetup(3,&DAC2Table,&SIUL.PGPDO[0].R,2,0,1,1,2,128,-256,0,EDMA_TCD_MODE_START);
I was also able to trigger the transfer of an array element using PIT and the triggered functionality. Nevertheless, I have again some problems in understanding how to use DMA with other modules.
It is really hard to get detailed information out of the reference manual and I didn´t found any application notes for the SPC56EL regarding this topic.
In DMA_MUX section, I saw the possibility to use the eTimer module as DMA source. Table 173 shows two sources for eTimer_0 - Channel0 and Channel1. But what does this mean? What kind of request connects the eTimer to DMA?Are they regarding to the capture and compare registers? And how do I use the eTimer in combination with DMA?
What I want to do is to trigger the transfer ofan array element when theeTimer produces a compare event. The eTimer should reload the load the new compare value from the compare load register, which should then be updated by DMA.
Best regards,
Patrik