User Activity

Hi !We are using an SR5E1E7. We want to put it as LockStep (both core and dma).So we have to setup the register 'Global System Configuration' / SYS_CFG_REG.We seen that we need to use the DCF.Do you have any example / file to setup this mcu like this...
Hi, We're testing an SPC58NN84E7 and encountering an issue with the ADC in DMA mode. Our debugger is an SPD5-UDESTK interfaced via OpenOCD.When inspecting the ADC's DMA result buffer through the debugger, all values appear valid. However, unexpected ...