ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST25R100 Tx power

I have successfully integrated a ST25R100 NFC reader with an ST25DV04K tag. Reading and writing data works perfectly.But once you enclose the system in its housing, writing doesn't work, even though reads still succeed.I presume this has something to...

X-nucleo nfc03a1 antenna measurement

Hi, I'm trying to measure X-Nucleo-nfc03a1 with VNA: i got completely different values for C11 C22 and C2 as is on nucleo board. I understood something wrong? and when I remove Resistors 330ohm, inductor and 4 100pF capacitors I got like: 

Andyb1_0-1770121215450.png Andyb1_1-1770121757457.png
Andy b1 by Associate II
  • 68 Views
  • 4 replies
  • 0 kudos

ST25R200 - (VDD_A to GND_A) capacitors

Hello.For example, on the datasheet of ST25R200, on page 10, it shows 2 capacitors between pins VDD_A and GND_A, but on page 13 it is not shown the recommended values of these 2 capacitors.Would they be 2.2uF and 10nF, or 1uF and 10nF, for example?I'...

jeferson by Associate II
  • 53 Views
  • 2 replies
  • 3 kudos

Resolved! ST25R100 NFC Tag Read Problems

Hi everyone,I’m trying to interface an ST25R100 NFC reader with my MCU, and I’m having trouble reading ISO15693 tags. My initialization seems to work, but I never get any response from the tag. I’m hoping someone can spot what I might be missing.This...