2021-03-23 10:38 AM
I'm trying to do a Project with the MAX30102. I can read out the raw data of the sensor but I am unable to understand the algorithm to calculate the Heartrate and SPO2 out of the raw data. The only examples I can find are for Arduino Boards but that's not useful at all. I found this one Example for the STM32F103C8T6 and I was hoping I could just convert it for my board so at least I got something that works...
Here is the link for the example:
https://www.programmersought.com/article/90827305857/
I have the code in the attachment.
I hope somebody can help me.
best regards,
F.Enis
2021-03-23 01:44 PM
Nice find but I see two problems:
How this will impact you if you don't use the KEIL compiler tool chain I have no idea
You should just use F466RE in Cube and try it! If you don't have the MAX30102 yet Adafruit has one and Mouser many - Mouser has the MAX Feather shield with the device.
FYI MAX has a repository on mbed with this device and mbed has the Nuleco-F446RE supported.
2021-03-24 04:24 AM
Thanks for the reply.
The problem is that I tried it but can't get anything to work.
I found this website: https://morf.lv/implementing-pulse-oximeter-using-max30100
The author is doing the processing for the MAX30100 but the same principles should apply for the MAX30102. The problem is that I have problems converting the code he used for my Project. I am not that good at programming to be honest.
I have my main file in the attachment. Maybe somebody could help me a little because I'm already really frustrated
best regards,
F.Enis
2024-09-29 11:42 AM
hey did u get ur output working?
2024-09-29 01:34 PM
From 3 years ago, try it yourself..
Read the data sheet. F1 and F4 are architecturally different. The HAL provides for a rough equivalence, and should be relatively fungible.