STM32 VSCode extension (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue with Linker Script in CubeMX 6.12.1

Dear users   After upgrading to STM32CubeMX 6.12.1 some of you reported limitations for CMAKE generated projects. We encourage you therefore to stick with the 6.12.0 for those encountering this limitation until the publication of the 6.13.0.    Thank...

New STM32 VSCode extension V2.1.0 released

Changelog Version 2.1.0 Added support for the following advanced STM32 devices TrustZone devicesDual Core devicesBootflash devices STM32CubeMX v6.12.0 is required to generate CMake projects for these advanced devicesSTM32CubeCLT v1.16.0 is required t...

vscode debug Global variables issue

Hello,I have a question about vscode with STM32 extension. I have setup a project with vscode and stm32 extension, and after compiler, it can do debug, and I can see the Global Variables on the VARIABLES window. as belowbut when I use vscode to do an...

dqsh06_0-1741858938092.png dqsh06_1-1741859152059.png
dqsh06 by Associate III
  • 337 Views
  • 0 replies
  • 0 kudos

TrustZone with VScode extension

Hi,I'm using an STM32L562 Discovery Kit, and trying to use the VSCode extension to debug.For now, I am only working with a basic code to blink LD10 with TrustZone activated.Now, I have an issue when flashing the MCU : the program doesn't seam to be r...

Adrian_ by Associate
  • 167 Views
  • 3 replies
  • 0 kudos

Resolved! CMake for TouchGFX via CubeMX?

Hi!Any chance this will be supported soon?CubeMX is already updating the auto generated CMake file in STM32 VS Code when adding TouchGFX but this is just for some of the TouchGFX files and is not sufficient, instead there will be build errors.As a re...

N6 VS Code launch.json for debugging

I'm having some difficulty getting debugging working in VSCode for the N6 series.  Does anyone have a sample one that actually works?  I'm obviously using the `stlink` server backend for `cortex-debug`, and I have tried using CubeIDE to get the exact...

JNT by Associate
  • 302 Views
  • 3 replies
  • 0 kudos

garbled characters in flash progress bar

quite a useful extension, it's much better than 1.x, yet there are still garbled characters with progress bar of task "flash(SWD)", in a lot computers, the progress bar is "圹"&“北”. I solved it by add "chcp 437" to task "flash(SWD)" in "lauch.json", b...

bonestan_1-1739968018347.png bonestan_0-1739968000884.png
bonestan by Associate
  • 121 Views
  • 0 replies
  • 0 kudos