/** \file max30102.h ****************************************************** * * Project: MAXREFDES117# * Filename: max30102.h * Description: This module is an embedded controller driver header file for MAX30102 * * * -------------------------------------------------------------------- * * This code follows the following naming conventions: * * char ch_pmod_value * char (array) s_pmod_s_string[16] * float f_pmod_value * int32_t n_pmod_value * int32_t (array) an_pmod_value[16] * int16_t w_pmod_value * int16_t (array) aw_pmod_value[16] * uint16_t uw_pmod_value * uint16_t (array) auw_pmod_value[16] * uint8_t uch_pmod_value * uint8_t (array) auch_pmod_buffer[16] * uint32_t un_pmod_value * int32_t * pn_pmod_value * * ------------------------------------------------------------------------- */ /******************************************************************************* * Copyright (C) 2016 Maxim Integrated Products, Inc., All Rights Reserved. * * Permission is hereby granted, free of charge, to any person obtaining a * copy of this software and associated documentation files (the "Software"), * to deal in the Software without restriction, including without limitation * the rights to use, copy, modify, merge, publish, distribute, sublicense, * and/or sell copies of the Software, and to permit persons to whom the * Software is furnished to do so, subject to the following conditions: * * The above copyright notice and this permission notice shall be included * in all copies or substantial portions of the Software. * * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS * OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF * MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. * IN NO EVENT SHALL MAXIM INTEGRATED BE LIABLE FOR ANY CLAIM, DAMAGES * OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, * ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR * OTHER DEALINGS IN THE SOFTWARE. * * Except as contained in this notice, the name of Maxim Integrated * Products, Inc. shall not be used except as stated in the Maxim Integrated * Products, Inc. Branding Policy. * * The mere transfer of this software does not imply any licenses * of trade secrets, proprietary technology, copyrights, patents, * trademarks, maskwork rights, or any other form of intellectual * property whatsoever. Maxim Integrated Products, Inc. retains all * ownership rights. ******************************************************************************* */ #ifndef MAX30102_H_ #define MAX30102_H_ //#include "mbed.h" #include "main.h" #define I2C_WRITE_ADDR 0xAE #define I2C_READ_ADDR 0xAF //register addresses #define REG_INTR_STATUS_1 0x00 #define REG_INTR_STATUS_2 0x01 #define REG_INTR_ENABLE_1 0x02 #define REG_INTR_ENABLE_2 0x03 #define REG_FIFO_WR_PTR 0x04 #define REG_OVF_COUNTER 0x05 #define REG_FIFO_RD_PTR 0x06 #define REG_FIFO_DATA 0x07 #define REG_FIFO_CONFIG 0x08 #define REG_MODE_CONFIG 0x09 #define REG_SPO2_CONFIG 0x0A #define REG_LED1_PA 0x0C #define REG_LED2_PA 0x0D #define REG_PILOT_PA 0x10 #define REG_MULTI_LED_CTRL1 0x11 #define REG_MULTI_LED_CTRL2 0x12 #define REG_TEMP_INTR 0x1F #define REG_TEMP_FRAC 0x20 #define REG_TEMP_CONFIG 0x21 #define REG_PROX_INT_THRESH 0x30 #define REG_REV_ID 0xFE #define REG_PART_ID 0xFF uint8_t maxim_max30102_init(void); uint8_t maxim_max30102_read_fifo(uint32_t *pun_red_led, uint32_t *pun_ir_led); uint8_t maxim_max30102_write_reg(uint8_t uch_addr, uint8_t uch_data); uint8_t maxim_max30102_read_reg(uint8_t uch_addr, uint8_t *puch_data); uint8_t maxim_max30102_reset(void); /* MAX30102_H_ */ #endif