2023-11-19 07:01 AM
Hi,
What am I missing ?
The connection to the event source is grayed and non selectable, see screen copies of the configuration below.
Solved! Go to Solution.
2023-11-20 06:09 AM - edited 2023-11-20 06:10 AM
here...
just rename txt to ioc . (ioc upload not allowed here - maybe STM dont know, what this ioc should be ...)
2023-11-19 08:04 AM - edited 2023-11-19 08:47 AM
i tried ...but: deselect external in comp
+ not select ext
-> if event4 not possible, use other event (1 or 2...)
try it.
2023-11-19 09:55 PM - edited 2023-11-19 09:56 PM
I initialized COMP2 and tried to select it: it is still grayed, -> something is preventing the selection.
On your side, it seems that you are starting from an already complex configuration (since PA0=COMP1_OUT was busy), could you try recreating a project from scratch, only selecting the processor G474 and configuring COMPx and HRTIM ?
Also I am using the latest cubeMX: 6.9.2, which version do you have ?
2023-11-19 10:58 PM - edited 2023-11-19 11:02 PM
ok... (in ide 1.13.1 ) + cube G4 1.51 (actual download) for G474RET6 :
i just set master timer on, not select any "external" in comp and hrtim event .
+
in your pic -> timer D has red cross -> you set something wrong there, clear this ! (cube shows you message, when mouse over the wrong item there , whats wrong)
2023-11-20 05:58 AM
Could you attach your .ioc file so I can peruse it ?
2023-11-20 06:09 AM - edited 2023-11-20 06:10 AM
2023-11-21 01:00 AM - edited 2024-01-28 06:17 AM
Thanks, resolved:
SOLUTION SUMMARY:
the trick is to *NOT* select "External event 4" in the upper "EXTERNAL EVENT LINES" topic but *enable* "External event 4" in the lower "External Event Configuration" pane.