2020-12-17 07:04 AM
Hi all, how are you?. I'm making a project with an STM32F401VE and I've updated the IDE, after that there are about ten dependencies that says something related to inknown dependencies and the .ioc project doesn't opens. I read some over there and some other people had the same problem after the STM32Cube IDE was updated, currently for me is showing this problem with the version Version: 1.5.1, Build: 9029_20201210_1234 (UTC).
I tried also to import the project or creating a new project but the behavior is the same. How could this problem be solved?
In the meantime I will simply reinstall the IDE
Solved! Go to Solution.
2021-01-15 07:34 AM
Hi,
My stm32cubeide 1.5.1 crashed after upgrading from the application (not able to build, "nature" problems like Johnny )
After uninstalling and installing 1.5.1 from scratch, I was able to build projects (imported and converted from old workspace)
After installing eGit, the problem came back again
2021-01-18 02:15 AM
i have the same problem with EGit and version 1.5.1.
When the plugin is installed stmcubeide crash.
i try reinstalling but it doesn't work.
Can anyone tell us how to solve it please.
2021-01-18 02:28 AM
ST has finally published 1.5.1 installers on www.st.com: STM32CubeIDE - Integrated Development Environment for STM32 - STMicroelectronics
Did you still get issue relying on it ?
Which OS are you relying on ?
2021-01-18 02:28 AM
ST has finally published 1.5.1 installers on www.st.com: STM32CubeIDE - Integrated Development Environment for STM32 - STMicroelectronics
Did you still get issue relying on it ?
Which OS are you relying on ?
2021-01-18 02:38 AM
last friday i downloaded that installer .
i installed it from scrath and the problem persist.
Im using Windows 10
2021-01-18 02:48 AM
I'm using Windows 10. I already used the 1.5.1 installer on Friday
2021-01-18 02:59 AM
The problem here is about the JRE version.
STM32CubeIDE embeds Java8 while, because of a 3rd-party installation (eGit, etc...), an indirect core dependency is updated and depends on Java11.
How to solve it
Notice: STM32CubeIDE has not been entirely validated on Java11, I strongly suggest to keep a backup of the jre folder.
2021-01-18 03:26 AM
thank you, this work for me
2021-01-24 11:05 PM
Thank you for the great support!
Sorry, next time I will check the ST Community first.
:thumbs_up:
2023-07-30 01:48 AM - edited 2023-07-30 01:49 AM
I have a similar warning: "Unknown referenced nature: fr.ac6.mcu.ide.core.MCUProjectNature"
I am unable to apply the fix as per @Julien D.
STM32CUbeIDE root has no jre/ subdirectory in my case (Windows10 64bit professional)
Current version (directory name 1.8.0 is remanent of first install)