STM32CubeIDE (MPUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 1.16.0 released

STM32CubeIDE 1.16.0 was released today on st.com as well as an in-tool update patch. What is new in 1.16.0?Microcontroller and board lists aligned with STM32CubeMX v6.12.0 : STM32C0 ,STM32WB0 and STM32MP25XXAdded CMake support for multicontext projec...

I have a Linux Computer with 6 dual threaded cores, which shows as 12 cores and 32 GB RAM. When I am running the IDE for the STM32MP1 it runs painfiully slow. Minutes to do things that used to take a second.

 am getting things like Multiple Problems have occurred. Compacting Resource Model. Refreshing Workspace, Workbench Autosave Job. An internal error occurred while showing an internal error. It says look at the .log file. I have not found where that i...

STM32CubeIDE Serial Console in use

I am stuck at step 6 inhttps://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4/Modify,_rebuild_and_reload_a_firmwareMPU Serial Console is operational, ethernet RJ45 also, and serial port ...

PeterL by Associate III
  • 1033 Views
  • 5 replies
  • 0 kudos

Resolved! I'm having trouble creating a project in STMCubeIDE 1.7.0. I'm trying to create the project in it's own directory, instead of the workspace directory. The process I am following is: (continued below)

- Create the directory for the project (C:\Project)- Create a New STM32 project- Select the processor and package- Setup STM32 project > Enter project name, for location enter project directory, select language and project type STM32Cube- Code Genera...

LThal.1 by Associate II
  • 644 Views
  • 5 replies
  • 0 kudos

How to debug M4 in production mode?

I am trying to Debug m4 in production mode. M4 is not halted.I am getting an error "Failed to insert breakpoint".I can successfully debug in Engineering mode. but, I need to Debug in Production mode.Can you explain how to solve this issue?

JSIGA.1 by Associate II
  • 585 Views
  • 6 replies
  • 0 kudos

Resolved! openSTlinux build from stm32cubeide to sdcard image

I've build all part (linux, tf-a, u-boot) in stm32cubeide, acording to my device tree configured in cube.I would like to ask if there is short way to create sd-card image from cube gui? If not, could any one share way how to do that from build to rea...

TStas.1 by Associate
  • 802 Views
  • 6 replies
  • 1 kudos