STM32CubeIDE (MPUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 1.16.0 released

STM32CubeIDE 1.16.0 was released today on st.com as well as an in-tool update patch. What is new in 1.16.0?Microcontroller and board lists aligned with STM32CubeMX v6.12.0 : STM32C0 ,STM32WB0 and STM32MP25XXAdded CMake support for multicontext projec...

Cannot debug CM4 on STM32MP151 (eng mode)

Both on Windows and on Linux, latest STM32CubeIDE, I cant get debug or run using ST-Link.If I try to use ST-Link GDB ServerError in final launch sequence: Failed to execute MI command: target remote localhost:61234 Error messa...

Resolved! Problem with DEBUG MCU STM32MP157A-DK1

I just created a project in STMCubeIDE for STM32MP157A-DK1 and am trying to run MCU debugging in ENGINEERING MODE and PRODUCTION MODE. I use an ST-LINK wire and an Ethernet Over USB connection. SSH and the UART command line work well. In engineering ...

How to include the library in the project correctly?

Good afternoon.I tried to create a demo project (STM32MP157C-DK2\Demonstrations\Al_Character_Recognition) for the STM32MP157D_DK1 board. When assembling, I had a problem.(Gluk_test_1) How to include the library in the project correctly? Sincerely, Al...

Vlaty.1 by Senior
  • 1261 Views
  • 13 replies
  • 0 kudos

The STM32CubeIDE debug failed

Hi, I am not newer for stm32cubeide. But the stm32cubeide had very bad experience on stm32mp1 platform. Most of the time the debug fails with the error prompt in the screenshot below. The solution is also just to reconnect the stlink or serial port.S...

0693W00000HpiEMQAZ.png
SChen.11 by Associate III
  • 429 Views
  • 1 replies
  • 0 kudos

Resolved! Decreasing RPMSG buffer size to 256 bytes on linux kernel will return "Failed to insert all hardware breakpoints.." when flashing or debugging M4 firmware from Cube IDE.

Hi there, I am trying to decrease the RPMSG buffer size from 512 to 256 bytes. I have successfully managed to increase the buffer size in the past to 1024 and allocate more memory for 32VRINGS. When attempting to decrease the buffer size to lower tha...

KChar.1 by Senior
  • 1034 Views
  • 4 replies
  • 0 kudos

When I try to program STM32MP157A-DK1 it says No ST-LINK detected. I tried to install 1.8.0 in Linux but it installed Version: 1.7.0 Build: 10852_20210715_0634 (UTC) instead.

The Nucleo F446RE pops up with a media directory as soon as I plug the USB into the ST-LinkThe STM32MP157A-DK1 does not do that. And when I try to program it it says NO ST-LINK Detected. I have tried the Boot switches in every position but I understa...