cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F767 ITCM Code Placement

TKana.1
Associate III

 

Hi,

I have been trying to place a function in the ITCM region for some time with no luck. As close I get was HardFalult There are some examples for the F7 series on the web. Some dating back to 2016, some similar to F767 with the same core but I cannot make them work. Each example uses a different way, making it harder to figure out. Modifying the linker file, modifying the startup.s file.

Yes, I read AN4667. 

I am using STM32CubeIDE 1.1.16. 

Is there a clear application note or up to date example code that I can use?

Best regards,

Tim

 

2 REPLIES 2
SofLit
ST Employee

Hello,

Maybe you can check this article it can help you: How to place and execute STM32 code in SRAM memory with STM32CubeIDE.

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

Hi,

I can run  from RAM without a problem but not from ITCM