2024-07-19 09:45 PM
Hi,
When using the .ioc to generate the code, it always shows:
- SMPS must be enabled to reach the best consumption figure. SMPS can be enabled from the Pinout tab under PWR
How to get rid of this? Or just omit it?
Solved! Go to Solution.
2024-07-19 09:57 PM - edited 2024-07-20 04:46 AM
Hello @diverger
Is just a message that containe some tips that may help the user to reduce consumption or in other cases to make the code work more Fluently or.... If you are not using them, you just have to omit them but you can't disble them. If you find this helpful, i will escalate your request to the Cube team so they may consider this recommandation to disable/enable those pop-ups in the comming releases.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-19 09:57 PM - edited 2024-07-20 04:46 AM
Hello @diverger
Is just a message that containe some tips that may help the user to reduce consumption or in other cases to make the code work more Fluently or.... If you are not using them, you just have to omit them but you can't disble them. If you find this helpful, i will escalate your request to the Cube team so they may consider this recommandation to disable/enable those pop-ups in the comming releases.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.