Skip to main content
Lukasz Nowak
Associate III
Nov 13, 2023 1:50 PM UTC
Solved

STM32U5 invalid SMPS warning during code generation

STM32CubeIDE 1.13.2 is showing a warning about SMPS for STM32U5 chips every time the code is generated (see attached).

This is done even for chips which do not have the SMPS pinout, e.g. STM32U595VJT (non Q), which is completely invalid.

But even when a chip does have SMPS, a designer may choose not to use it - why does this warning have to be shown every time the code is generated?

For reference CubeMX used in this version of IDE is:

Version: 6.9.2-RC4
Build: 20230910-1412 (UTC)

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Nov 16, 2023 3:58 PM UTC

Hello again @Lukasz Nowak 

After check, I confirm that CubeMX should not allow to select the SMPS option in STM32U59xx device without SMPS.
Issue is reported internally to our team (Internal ticket number: 166485) and this will be fixed as soon as possible.

(PS: ID166485 is an internal tracking number and is not accessible or usable by customers)

PS: Issue solved on the last release of the STM32CubeMX

Thank you for reporting that.

Best Regards.

STTwo-32.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

STTwo-32
ST Technical Moderator
Nov 13, 2023 2:05 PM UTC

Hello @Lukasz Nowak and welcome back to the ST Community :smiling_face_with_smiling_eyes:.

Thank you for reporting this. I will check it internally and get back to you as soon as possible.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Nov 16, 2023 3:58 PM UTC

Hello again @Lukasz Nowak 

After check, I confirm that CubeMX should not allow to select the SMPS option in STM32U59xx device without SMPS.
Issue is reported internally to our team (Internal ticket number: 166485) and this will be fixed as soon as possible.

(PS: ID166485 is an internal tracking number and is not accessible or usable by customers)

PS: Issue solved on the last release of the STM32CubeMX

Thank you for reporting that.

Best Regards.

STTwo-32.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.