Skip to main content
Senior
Jul 20, 2024 4:45 AM UTC
Solved

NUCLEO-U5A5ZJ-Q 'SMPS must be enabled to reach the best consumption figure'

Hi,

When using the .ioc to generate the code, it always shows:

- SMPS must be enabled to reach the best consumption figure.   SMPS can be enabled from the Pinout tab under PWR

How to get rid of this? Or just omit it?

    This topic has been closed for replies.
    STTwo-32
    STTwo-32Best answer
    ST Technical Moderator
    Jul 20, 2024 4:57 AM UTC

    Hello @diverger 

    Is just a message that contain some tips that may help the user to reduce consumption or in other cases to make the code work more Fluently or.... If you are not using them, you just have to omit them. But you can't disable them. If you find this helpful, I've escalated your request (in the internal ticket number 187848) to the Cube team so they may consider this recommendation to disable/enable those pop-ups in the coming releases.

    Best Regards.

    STTwo-32 

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    9 replies

    STTwo-32
    STTwo-32Best answer
    ST Technical Moderator
    Jul 20, 2024 4:57 AM UTC

    Hello @diverger 

    Is just a message that contain some tips that may help the user to reduce consumption or in other cases to make the code work more Fluently or.... If you are not using them, you just have to omit them. But you can't disable them. If you find this helpful, I've escalated your request (in the internal ticket number 187848) to the Cube team so they may consider this recommendation to disable/enable those pop-ups in the coming releases.

    Best Regards.

    STTwo-32 

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Texram
    Associate III
    Jul 29, 2024 11:01 PM UTC

    Hi STTwo-32,

    I'm using CubeMX 6.10.0 and try to configure STM32U575.

    I keep getting this message and don't see any option to enable SMPS under PWR

     

    Texram_0-1722293946394.png

    Texram_1-1722294032298.png

     

    BarryWhit
    Lead
    Jul 30, 2024 1:50 AM UTC

    @Texram , there are two bugs here:

    1. Cube gives you the warning about enabling the SMPS even for STM32U5 parts which do not contain an SMPS.

    (can't reproduce this now, I must have confused projects with diff part numbers when checking this)

    2. If the part does include an SMPS (part number includes a Q suffix), the UI buries the SMPS enable option 5 levels down:

    SMPS.jpg

     

    Now that's some mighty terrible UX right there.

     

    I've started this bug-report thread

     

    "- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."
    Texram
    Associate III
    Jul 31, 2024 1:46 AM UTC

    Thanks for the info, BarryWhit.

    BarryWhit
    Lead
    Jul 31, 2024 4:44 PM UTC

    @Texram , could you tell me which specific U575 you're working with and what CubeIDE version you're using? I thought I saw (bug 1) above, but I can't reproduce it now that ST has asked me to. Does your project use a xxxQ (i.e. with SMPS) part number?

    "- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."
    ST Technical Moderator
    Aug 1, 2024 9:52 AM UTC

    Hello @BarryWhit ,

    Further to your comment, the SMPS is well removed from configuration of Power Saving Mode.

    [ STM32U595xxxx] ; [STM32CubeMX 6.12.0]

    We still have a waring Mentioned above.

     

    MahmoudBenRomdhane_0-1722505321506.png

    In fact, this problem has already been reported internally to the development team through ticket 166502.

    Thanks.

    Mahmoud

     

     

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    BarryWhit
    Lead
    Aug 1, 2024 10:57 AM UTC

    @Mahmoud Ben Romdhane wrote: 

    Further to your comment, the SMPS is well removed from configuration of Power Saving Mode.

    [ STM32U595xxxx] ; [STM32CubeMX 6.12.0] 


    @Mahmoud Ben Romdhane , I'm not sure I understand you. What exactly do you mean by "the SMPS is well removed from configuration"? 

     

    Thank you for confirming that STM32U595 parts lacking SMPS do indeed erroneously show the warning message. Glad to learn I wasn't hallucinating after all.

    "- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."