cancel
Showing results for 
Search instead for 
Did you mean: 

Need help configuring SDIO to read SD card on STM32F405 using STM32CubeIDE.

DLim.16
Associate II

Hi,

I am trying to use the STM32F405 microcontroller to log data into an SD card using STM32CubeIDE. Specifically, this MCU from adafruit: https://www.adafruit.com/product/4382?gclid=EAIaIQobChMI3qONnpCJ5wIVD_DACh2XCQY7EAAYASAAEgL4QvD_BwE

I found a few resources online and integrated that into the my source code, which can be found in "main.zip". My SDIO and FATFS configurations are shown in the attached figures. I did not change anything under 'Set Defines'.

Regardless of whether I have an SD card in the MCU or not, the results are the same: the program doesn't go beyond the line of code that calls "f_mkfs". I would appreciate it if someone could help me troubleshoot this.

Thanks.

18 REPLIES 18

Formatted cards should not need MKFS, one should avoid using it at all until DISKIO layer read function is fully tested/validated.

Unfortunately I lack the will to trawl through broken code, especially from Cube.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
DLim.16
Associate II

Hi clive1,

Thank you for your answer!

I removed "f_mkfs" and my program gets stuck in the next line of code, which is 'f_open'. It fails to open/create a file.

Also, what did you mean by "until DISKIO layer read function is fully tested/validated"? How can I test/validate that function?

Thanks.

dbgarasiya
Senior II

you are missing sd card initializartion and configuring of bus width functin missing in you project

and according to @Community member​  , you do not need to use f_mkfs

Hi Dbgarasiya,

I thought the IDE already initialized the module after configuring it using the GUI in Device Configuration Tool. It even created a function call: 'MX_SDIO_SD_Init'.

Do you think maybe the module wasn't initialized properly? If so, what are the right function calls I should be using?

Thanks.

dbgarasiya
Senior II

BSP_SD_Init()

dbgarasiya
Senior II

bsp_driver_sd.c in this file

Hi Dbgarasiya,

I added that, but I am still getting the same result. Am I missing something else?

Thanks.

dbgarasiya
Senior II

you have not enable DMA, for rx and tx also

then try

Hi Dbgarasiya,

Looks like I can only choose to either use SDIO or SDIO RX & TX but not all three of them, otherwise I get an error say "No available DMA requests for this peripheral".

Was DMA required? I enabled both variations i.e. only SDIO and then only SDIO RX & TX, nothing worked. Let me know if I'm doing something wrong.

Thanks.