2024-10-31 5:05 PM
Hi.
I'm aware that there's a cli tool called STM32CubeCLT which is used for building programs for stm32 MCUs.
But, is there any way that we can ask stm32cubeIDE to perform the following steps?
To give a bit of context:
We're making cmsis pack to deliver software components to stm32cubeIDE and we'd like to automate the process of testing each pack in our CI/CD.
2024-11-01 9:16 AM
Hello @miladmohtashamirad
Currently, it is not possible to perform certain actions on the cmsis-pack with STM32CubeCLT. However, CubeCLT allows:
• Building a program for STM32 MCU devices using an enhanced GNU toolchain for STM32
• Programming STM32 MCU internal memories (flash memory, RAM, OTP, and others) and external memories
• Verifying the programming content (checksum, verification during and after programming, comparison with file)
• Automating the STM32 MCU programming
• Debugging applications through the interface of STM32 MCU products, which provides access to MCU internal resources using basic debug features
Thx,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.