STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 441 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 323 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Unable to Download FlashLayout_sdcard_stm32mp157f-dk2-trusted.tsv using STM32 CubeProgrammer on Win10 host PC

 I'm trying to download Starter Package to microSD card on STM32MP157F-DK2 via USB.I clicked "Open file", selected "FlashLayout_sdcard_stm32mp157f-dk2-trusted.csv", pressed RESET button, clicked "connect" and tried to download.​However, STM32CubeProg...

0693W00000Nro2FQAR.png 0693W00000Nro2eQAB.png
skawa.1 by Associate
  • 1545 Views
  • 1 replies
  • 0 kudos

STM32CubeProgrammer fails with: "Error: Message from Embedded Flash Loader : Layout line 1: invalid option '¸' in ¸)"

Hi community,I'm facing problems to upload the flash layout on a custom board with the STM32CubeProgrammer. I tried with the last version (v2.10.0) but also older ones. The USB communication seems to be working fine as there are not checksum errors o...

STM32CUBE IDE STM32MP1 Debugging Error

Hi all,I am trying to debug an C++ user space application on A7using STM32CubeIDE.Build happens fine. But when i try to debug it i run into following errors.I can confirm the toolchain is installed both on system as well as embedded in CUBEIDE.How ca...

NPal.2 by Senior
  • 2115 Views
  • 1 replies
  • 0 kudos

Resolved! Is SWCLK required for SWD ?

The four wire interface from the ST-LINK V2 has no clock.Where does it say that ST devices do not require a clock for SWD ?Also why is it seemingly impossible to work through a hub ? This makes life very difficult.

JSchn.5 by Associate III
  • 3008 Views
  • 3 replies
  • 0 kudos