| Subject | Author | Posted | |
|---|---|---|---|
| 2026-05-14 11:10 PM | |||
|
Due to absence of a security forum for MPU's (while there is for MCU's) posting this here. The CRA...
| 2026-05-05 6:20 PM | ||
|
Hello everyone, I'm a beginner in the STM32 world, A teacher has lent us a STM32MP157C-DK2 boar...
| 2026-03-06 8:00 AM | ||
|
I'm working on STM32MP257F-DK board. I use a device tree without SD card, only eMMC. I set BOOTDEVI...
| 2026-02-25 7:38 AM | ||
|
Hello, I'm trying to install EGit in STM32CubeIDE, but I'm getting an error. Cannot comple...
| 2026-02-22 9:13 AM | ||
|
Hello, A question on STM32CubeMX v6.16.1, when I select OpenAMP in Middleware and Software Packs,...
| 2026-02-19 9:55 AM | ||
|
Hi, I am trying to enable secure boot in STM32mp157f-ev1 board. I am using the Developer Package s...
| 2026-02-12 6:21 AM | ||
|
This post provides a workaround for a specific issue in STM32CubeIDE v2.0.0. The issue will be reso...
| 2025-12-11 8:48 AM | ||
|
Hello, I'm trying to modify STM32MP157x-DK2 kernel so that it would use ST ethernet drivers (dwmac...
| 2025-12-08 1:02 PM | ||
|
Description: When configuring DDR parameters for STM32MP257 in STM32CubeMX, I changed the DDR s...
| 2025-11-14 12:24 AM | ||
|
Using CubeMX v6.15 on Windows 11 I tried generating a project for MP257-EV1 selecting the M33-Mast...
| 2025-11-13 5:23 PM | ||
|
使用千问大模型询问STM32MP157使用docket +vscode开发调试方式,它说VSCODE目前(大模型只能判断到2024初的信息)只支持A7用gdb调试,而M4只能用stlink+离线版的...
| 2025-11-07 2:15 AM | ||
|
Hello everyone, I’m using an STM32MP157F-DK2 board and trying to use one of the Cortex-M4 debuggin...
| 2025-10-27 11:02 PM | ||
|
I just bought STM32MP135F-DK and tried to build a HelloWorld project using STM32cubeIDE File->New>...
| 2025-10-23 7:58 AM | ||
|
When a STM32MP2 is "USB/UART for programming" mode i.e. all boot switchs off. I am running Ubuntu ...
| 2025-10-08 4:33 AM | ||
|
Hi, Since the STM32CubeIDE "Target status widget" for some reason isn't receiving the IP address ...
| 2025-09-23 11:08 AM | ||
|
Hi, I followed the steps in the link below, minus "populate target," but I was able to successfull...
| 2025-09-21 10:34 AM | ||
|
Hello everyone. I'm developing a bare metal project on STM32mp135F-DK using Keil RTX5 operating sy...
| 2025-08-27 1:03 AM | ||
|
Im trying to enable x11 feature in yocto build for stm32mp257f-ev1, im getting error while compilin...
| 2025-07-31 9:26 PM | ||
|
I've upgrade an ioc based project for the STM32MP157F-DK2 from CubeIDE 1.18 to 1.19 and from Ecosys...
| 2025-07-23 6:50 AM |