STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 442 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 323 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

#include <gtk/gtk.h> in STM32IDE issue

I've followed this:https://www.youtube.com/watch?app=desktop&v=qEzfqKt3exE&list=PLnMKNibPkDnFp5YvrvWjgfjrOs0Vi34Mt&index=5and set up project in STMCUBEIDEwhen i try and include #include <gtk/gtk.h> i get the followingmake all Wrapper for /opt/st/stm3...

RSmit.11 by Associate
  • 1573 Views
  • 1 replies
  • 0 kudos

Cannot debug CM4, "Unable to create ... because of "java.io.IOException: inputstream is closed"

I'm trying to program/debug a CM4 co processor on a STM32MP151 3rd party board.I setup the Debug as "thru Linux core" Serial port and Inet address looks ok, I got a green connection light, "status connected", and after trying to debug, I got this mes...

Resolved! In a later step we plan to flash several chips in parallel on one Windows host system. For this it is necessary to be able to assign connected boards clearly.

External memory, connected to a STM32MP1, is written with the STM32CubeProgrammer via USB. Here the chip to be written is written with "usb1" (STM32_Programmer.sh -c port=usb1 -d some.tsv").Here we could notice the following behavior: If more than on...

_MHeuc.1 by Associate
  • 2427 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeProgrammer - Segmentation fault (SIGSEGV) when trying to connect to a STM32MP157F-DK2 via SWD/JTAG

When I try to connect to a STM32MP157F-DK2 board via SWD/JTAG, STM32CubeProgrammer aborts with a segmentation fault on my host system (openSUSE Leap 15.2).I get the following error message, when I start STM32CubeProgrammer within a shell:# # A fatal ...

krjdev by Associate II
  • 5514 Views
  • 6 replies
  • 0 kudos