STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 441 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 323 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

CubeProgrammer shows that partition size is negative, fail to program using CubeProgrammer (kernel panic), but successful with raw SD card image using Win32DiskImager

Hi everyone,I have a problem using STM32CubeProgrammer (and CLI). They are both showing that my userfs partition have a size of -1162381824 bytes. That partition have size of 2.9GB. After programming with CubeProgrammer I have kernel panic, and I don...

0693W000007ZBa9QAG.png
NGajic by Associate III
  • 2998 Views
  • 6 replies
  • 0 kudos

Resolved! What is the layout of the .tsv file?

I'm updating a .tsv file, used by the CubeProgramer to program a STM32MP DK1. The file I'm looking at contains:#Opt Id Name Type IP Offset Binary - 0x01 fsbl1-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157a-dk1-serialboot.stm32 - 0x03 ssbl...

MWors.1 by Associate II
  • 2964 Views
  • 3 replies
  • 0 kudos

How can i enable SPI5 on STM32MP157-DK1

Hi,Im working with STM32MP157A-DK1 board. Im working on the linux side, need to write C/C++ code for saving data into a SD card. I need to use SPI to get data from RF transceiver. I built linux and kernel as in this link:https://wiki.st.com/stm32mpu/...

MÇerçi by Associate III
  • 3239 Views
  • 3 replies
  • 0 kudos

STM32MP157C-DK2 M4 debugging issues.

Hi, I have 10 DK2's in a server rack for development and testing. STM32CubeIDE (1.5.0) debugging wants me to specify a serial port and an IP address for debugging. This is IMHO redundant, why? Moreover, the serial ports /dev/ttyACM* are to be selecte...

KnarfB by Super User
  • 1791 Views
  • 2 replies
  • 0 kudos