Skip to main content
Dub Bartolec
Associate III
July 25, 2025
Question

STM32MP157-EV Debugging and running code on M4 from STM32CubeIDE and Win11

Hi All,

We've tested debugging of M4 code on STM32MP157-EV using STM32CubeIDE from native Ubuntu linux.
It all works as expected as it was documented here: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4/Modify,_rebuild_and_reload_a_firmware

We've also tried the same on STM32CubeIDE running on Win11 computers. And it all worked fine for some and not for others. E.g. On some laptops it works OK but on others it doesn't let us select "MPU Serial" console even it was recognized as STLink Virtual Port.

E.g. This is an example of working setup on Laptop1:

DubBartolec_0-1753407286649.png
And this is an example of how it doesn't work on another laptop Laptop2 :

DubBartolec_1-1753407395754.png

As it is clear Win11 correctly detected ST-Link Virtual UART but it is not showing in STM32CubeIDE as it does on other laptop. We tried it on several laptops and it worked on some and doesn't on others.

Versions of STM32CubeIDE we were running were 1.18 and 1.19 but no differences. It always works OK on some computers but never on another.

Has anyone noticed similar behaviour ?

4 replies

Ghofrane GSOURI
ST Technical Moderator
August 11, 2025

Hello @Dub Bartolec 

First, thank you for sharing your issue.

Could you please provide the log file from the computer where the problem was observed? You can find the log in the .metadata folder within your STM32CubeIDE workspace directory. This information will help us better understand and troubleshoot the issue.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
September 5, 2025

sorry for hijacking this thread... but here is the snippet of ".log" file from my setup..

!ENTRY com.st.stm32cube.ide.mpu.remote.serial 4 0 2025-09-05 13:28:12.268
!MESSAGE Failed to parse wmic output
!STACK 0
org.xml.sax.SAXParseException; lineNumber: 1; columnNumber: 1; Premature end of file.
	at java.xml/com.sun.org.apache.xerces.internal.parsers.DOMParser.parse(DOMParser.java:262)
	at java.xml/com.sun.org.apache.xerces.internal.jaxp.DocumentBuilderImpl.parse(DocumentBuilderImpl.java:342)
	at com.st.stm32cube.ide.mpu.remote.serial.internal.SerialPortProviderWindows.run(SerialPortProviderWindows.java:127)
	at java.base/java.util.TimerThread.mainLoop(Timer.java:566)
	at java.base/java.util.TimerThread.run(Timer.java:516)

!ENTRY com.st.stm32cube.ide.mpu.remote.serial 4 0 2025-09-05 13:28:13.280
!MESSAGE Failed to parse wmic output
!STACK 0
org.xml.sax.SAXParseException; lineNumber: 1; columnNumber: 1; Premature end of file.
	at java.xml/com.sun.org.apache.xerces.internal.parsers.DOMParser.parse(DOMParser.java:262)
	at java.xml/com.sun.org.apache.xerces.internal.jaxp.DocumentBuilderImpl.parse(DocumentBuilderImpl.java:342)
	at com.st.stm32cube.ide.mpu.remote.serial.internal.SerialPortProviderWindows.run(SerialPortProviderWindows.java:127)
	at java.base/java.util.TimerThread.mainLoop(Timer.java:566)
	at java.base/java.util.TimerThread.run(Timer.java:516)

!ENTRY com.st.stm32cube.ide.mpu.remote.serial 4 0 2025-09-05 13:28:14.267
!MESSAGE Failed to parse wmic output
!STACK 0
org.xml.sax.SAXParseException; lineNumber: 1; columnNumber: 1; Premature end of file.
	at java.xml/com.sun.org.apache.xerces.internal.parsers.DOMParser.parse(DOMParser.java:262)
	at java.xml/com.sun.org.apache.xerces.internal.jaxp.DocumentBuilderImpl.parse(DocumentBuilderImpl.java:342)
	at com.st.stm32cube.ide.mpu.remote.serial.internal.SerialPortProviderWindows.run(SerialPortProviderWindows.java:127)
	at java.base/java.util.TimerThread.mainLoop(Timer.java:566)
	at java.base/java.util.TimerThread.run(Timer.java:516)

!ENTRY com.st.stm32cube.ide.mpu.remote.serial 4 0 2025-09-05 13:28:15.268
!MESSAGE Failed to parse wmic output
!STACK 0
org.xml.sax.SAXParseException; lineNumber: 1; columnNumber: 1; Premature end of file.
	at java.xml/com.sun.org.apache.xerces.internal.parsers.DOMParser.parse(DOMParser.java:262)
	at java.xml/com.sun.org.apache.xerces.internal.jaxp.DocumentBuilderImpl.parse(DocumentBuilderImpl.java:342)
	at com.st.stm32cube.ide.mpu.remote.serial.internal.SerialPortProviderWindows.run(SerialPortProviderWindows.java:127)
	at java.base/java.util.TimerThread.mainLoop(Timer.java:566)
	at java.base/java.util.TimerThread.run(Timer.java:516)
Ghofrane GSOURI
ST Technical Moderator
October 16, 2025

Hello @Nisarg @Dub Bartolec 

Could you please provide me with the output of the following command from your command prompt (cmd)?

wmic path Win32_PNPEntity WHERE "Name LIKE '%%(COM%%'" get Name,Manufacturer /format:rawxml


Additionally, please test the same scenario using a fresh installation of CubeIDE 1.17.0 and let me know whether you can reproduce the same behavior.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.