Resolved! Is there a way to load more than one file at a time in automatic mode using STM32CubeProgrammer?
I want to load a bootloader and then the firmware to my board via ST Link in one pass in an automatic mode.
I want to load a bootloader and then the firmware to my board via ST Link in one pass in an automatic mode.
I work on Windows and use the STM32CubeIDE 1.6.1. I want to program and debug the M4 part, On the A7 part Linux is working.My current state is, that The A7 is in Bootloader mode and the DFU per USB is connected and shown in Windows (Gerätemanager) a...
I can't connect to my STM32MP157 evalaution board. I have installed required libraries as decribed in the tutorial: https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package 5.1 Installing the STM32CubeProgrammer tool. However I g...