STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Power sequencing inconsistency

quote from hardware development application note -"VDD3V3_USBHS must not be present unless VDDA1V8_REG is present, otherwise permanentSTM32MP15x lines damage can occur. It must be ensured by PMIC ranking order or withexternal component in case of dis...

QtMultimedia with PyQt5

Hi st team,I tried to used Qtmultimedia with PyQt5 i clone in layers meta-qt5 and meta-st in meta-st i used meta-st-x-linux-qt and completed build.Build Configuration:BB_VERSION = "2.4.0"BUILD_SYS = "x86_64-linux"NATIVELSBSTRING = "universal"TARGET_S...

rajsingh by Associate
  • 415 Views
  • 1 replies
  • 0 kudos

Resolved! MP2, ADC and noise

Hello,I plan to use a MP2 on a SOM module (probably something like the KaRo QFN-like QSMP2 module).This MP will run a linux on the A35 core and real-time software on the M33, + USB2, ETH 100 Mbps.I need 11 ADC channels to convert analog signals at 50...

tarzan2 by Senior
  • 680 Views
  • 2 replies
  • 1 kudos