STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! auto-mount a USB

 "is there possibility we can auto mount a usb when connected to usb host and how to build the udev-extraconf package for my stm32mp157f-dk2" how to build this   please give the steps to build for my stm32mp157f-dk2 as i want my pendrive to mount aut...

Sharan by Senior II
  • 1225 Views
  • 1 replies
  • 0 kudos

STM32MP257 Programming

I have had difficulties programming the STM32MP257 via stm32cubeide. I followed the first few steps to flash an OS image onto the board using the section populate and boot the image, from the STM website. When trying to flash IOC generated code via s...

mtc65536 by Associate II
  • 1097 Views
  • 1 replies
  • 2 kudos

Resolved! stm32mp15x dfu over usb not detected

Dear All,I'm having problem to get DFU over USB running on custom board.In general device can boot from SD card and with no SD card it can be detected via uart4 by STM programmer, so it enters DFU as far as I can tell.USB DP/DM is connected to DP2 (b...

OskarM by Associate III
  • 964 Views
  • 1 replies
  • 0 kudos

Resolved! STM32DDRFW-UTIL failed

 Hello,I am testing a custom board based on STM32MP257FAK3 with two DDR4 MT40A1G16RC-062E_B devices, for a total of 4 GB (32-bit width).I have correctly set up the main configuration files to work with the PMIC and UART. I also exported the PCB layou...

jcalvo_0-1757945405655.png
jcalvo by Associate II
  • 1458 Views
  • 5 replies
  • 0 kudos