STM32 MPUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Do you know MPU Wiki User Guide ?!

You have a question regarding STM32MP1 product and its ecosystem ? There is a good chance you find it in the MPU Wiki User Guide (https://wiki.st.com/stm32mpu ) This user guide aims at assisting developers to use STM32 MPUs microprocessor devices fr...

Resolved! to exit low power mode - stm32mp157c

Hello,I read the related wiki page and low power mode document.I can enter low power mode with the command "echo mem > /sys/power/state". Thats great.My M4 program is still running in the background. I am reading a sensor in this program. If it reads...

IYetk by Associate III
  • 649 Views
  • 2 replies
  • 0 kudos

is there an easy and convenient way of updating rootfs

i mean do the update somehow on the fly without removing the card from a running system, on the pc build a new rootfs and instead of removing the card, and do the copying on the pc, do this directly on the dk board. in principle it should be possible...

STM32MP1 BootLin BlogPost

Dear STM32 MPU Community,Please find below some technical STM32MP1 BlogPost from our partner Bootlin :https://bootlin.com/blog/building-a-linux-system-for-the-stm32mp1-basic-system/https://bootlin.com/blog/building-a-linux-system-for-the-stm32mp1-co...

KKHOL by ST Employee
  • 867 Views
  • 3 replies
  • 6 kudos

Resolved! PANIC during wake up MPU

Hello.I have a DK2 board and I want to wake up MPU (CA7) after shutdown command. If no MCU (CM4) firmware is running then no problems, but otherwise if I run MCU firmware (GPIO example) before shutting down MPU I get the following error after pushing...

alexey.b by Associate II
  • 973 Views
  • 2 replies
  • 0 kudos

Resolved! Initramfs: chip reboots after 30s seconds

Hi,I'm playing around initramfs shell using initramfs-framework in Yocto environment.I found that the chip abruptly reboots after some time (I think it's around 30 seconds) if the initramfs doesn't fully boot the system by entering systemd.I think it...