STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Force re-compile local kernel changes

Hi,I have done certain changes to support the display in the dts files.I have modified dts files under kernel and u-boot.I had also added certain changes in panel-simple.c file as well. I gave a build and forgot to make some changes. So i changed tho...

NPal.2 by Senior
  • 1873 Views
  • 6 replies
  • 0 kudos

Resolved! Is there a way to load U-boot on STM32MP1 via dfu-util instead of STM32CubeProgrammer?

I want to use open source utilities to load U-boot into SRAM in "Serial mode". Is it possible?P.S. As I can see, there is an article about it on ST Wiki, but an access to it is restricted for regular users: https://wiki.st.com/stm32mpu/wiki/How_to_lo...

SNaza.1 by Associate
  • 1038 Views
  • 4 replies
  • 0 kudos

Resolved! Linux SDK for ARM

Is there also an ARM version of the SDK to develop the Modules.because here I only found a X86 versionhttps://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package#Installing_the_SDK

SAman.1 by Associate III
  • 2205 Views
  • 6 replies
  • 2 kudos

Resolved! How to disable STM32MP1 cortex M4 core

We are using a STM32MP157 chip on a custom low-power design and don't need the Cortex M4 core. We would like to disable it properly to reduce power consumption and also remove dedicated support in linux kernel.Is there any recommended way to do this ...

PGE by Associate III
  • 1726 Views
  • 5 replies
  • 0 kudos

Resolved! STM32MP157 not exiting suspend to Linux

We are seeing some strange behavior on our stm32mp157 system exiting suspend mode.This is not a 'weston' build, so we enter (deep) suspend mode by executing "echo mem > /sys/power/state" and the system powers down and enters low power.root@stm32mp157...

drew by Associate III
  • 3202 Views
  • 7 replies
  • 0 kudos

Resolved! LVDS Display Troubleshooting

Hi all,I am trying to bring a LVDS display up. Display: BOE EV121WXM-N10-1850. Datasheet: LinkDriving MPU : STM32MP1. I am using VisionSoM STM32MP1 based evaluation Kit. LinkThe firmware changes required to make the device up are part of git: LinkI h...

NPal.2 by Senior
  • 1834 Views
  • 2 replies
  • 0 kudos