STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Image install to emmc using sd card

Hello GuysI'm using a157-EV1 board and my custom board.Both board have sd card slot and emmc. And possible of linux install to sd card and emmc.Anyway if built images using STM32_Programmer_CLI in Ubuntu environment can be install on the board accord...

SPark.15 by Associate II
  • 9032 Views
  • 5 replies
  • 0 kudos

Support of signing and validation mechanism of kernel and filesystems in stm32mp157f-eval board

Hi STM-Team,I am working with STM32MP157F-Eval board. I have enabled and tested secure-boot flow as per https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_secure_boot.Now, I am looking for next security part for singing-verification of kernel & DTB...

Resolved! Hello, i'd like to use u-boot command sspi to send commands to a spi device with a custom protocol (not a memory). However I see that the command tries to read an ID as it is talking to a flash nor : unrecognized JEDEC id bytes: 00, 00, 00.

Looking at the code, i see file sf_probe.c with .id      = UCLASS_SPI_FLASH, that performs the id reading. How can i use stm32_spi.c with .id         = UCLASS_SPI, driver instead? and send "raw" spi data?

Lmoio.1 by Senior
  • 8998 Views
  • 8 replies
  • 0 kudos

Resolved! Hello, I've exported our custom root filesystem from a running board with the following command: dd if=/dev/mmcblk1p4 of=/usr/local/rtfs.ext4 bs=1M conv=fdatasync

I noticed that after I flash the ST starter package root filesystem, at first boot there is a check on bad blocks and a resize of the partitions, while when I flash the exported root filesystem, there is no checks and some partitions are not resized ...

Lmoio.1 by Senior
  • 3795 Views
  • 5 replies
  • 0 kudos