STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LAN8720 Custom SOM Issue

We have custom SOM which has been designed with STM32MP157C.We are using the OpenSTLinux 3.0.0 as of now as the distribution running on it.In case of LAN PHY interfacing we are using LAN8720.There is a strange behavior , upon I can see the below mess...

0693W00000Hr4uWQAR.png
NPal.2 by Senior
  • 1086 Views
  • 3 replies
  • 0 kudos

Resolved! ADC sampling from ANA0/ANA1 via M4

Hi,I have some doubts about how I could sample from the ANA0/ANA1 pins of an STM32MP1 CPU from inside the M4 firmware via HAL. I would like to programmatically switch between these two pins.Sampling from ADC_CHANNEL_0 seems to work, so I guess it is ...

ATringali by Associate II
  • 1795 Views
  • 4 replies
  • 0 kudos

STM32NP157D Discovery Kit Getting Started: Kernel rebuild example hangs: ERROR: reserving fdt memory region failed (addr=d4000000 size=4000000) Any ideas?

I am evaluating the STM32NP157D Discovery Kit.In the Getting Started Section I have successfully done the gtk_hello_world step.The next step successfully rebuilds the kernel. After pushing it on the board I do the reboot and get the following Error m...

RTjep.1 by Associate
  • 871 Views
  • 0 replies
  • 0 kudos