Resolved! Can STM32MP151FAA1 support WinCE OS?
Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
*** The source tree is not clean, please run 'make ARCH=arm mrproper'*** in /home/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10***make[2]: *** [outputmakefile] E...
HelloI have problem, i can't flash emmc on SoM MYC-YA157C-V2 (STM32MP157A).I use STM32CubeProgrammer ver.2.11.0 under Windows 11 OS.Tried to use STM32CubeProgrammer and _CLI (with different wait timeouts).My firmware script:set tsv="FlashLayout_emmc_...
Hi,root@si-rd22:/home/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-2020.10.r1-r0/u-boot-stm32mp-2020.10.r1# make stm32mp15_defconfigMakefile:40: *** missing separator. Stop.can anyone ...
Hi,We are using SEEED studio 102110318 module which uses STM32MP157CAC3 processor. We want to know if there is any way we can keep processor pin PD13 pin to low state in suspend state. We want the pin to maintain low state while in sleep mode. We hav...
I want to use arm-ostl-linux-gnueabi-gcc on windows. I have installed stm32mp1-gcc9.3.0-r2.exe on my windows 10 OS. When I try to compile a code, libraries like stdlib.h etc not found error appears. How can I resolve this?
Hi.I am following the instructions written in STM32MP1 Developer Package - stm32mpu and meta-st-stm32mp/README.HOW_TO.txt at kirkstone · STMicroelectronics/meta-st-stm32mp · GitHub to build u-bootWhen I execute make -f $PWD/../Makefile.sdk all, I get...
Hi ST experts,Would like to check if STM's MPU able to support Window CE 6 or Linux platform?Thank you
Hi!Problem: The board boots correctly into the Linux kernel, but the kernel is unable to mount the rootfs.We designed a custom board using stm32mp157f. It is based on the DK2 with some differences:PLL Base clock 48Mhz (instead of 24MHz)Other power su...