STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Compilation breaking on custom machine

In the recently, for the past few days, I am facing this new issue that, if i compile for my custom som and program, i always get this error. But if I dont do any add-on of packages, I works fine.I even added a simple package like "vim" using IMAGE_I...

NP by Associate II
  • 7270 Views
  • 5 replies
  • 0 kudos

Issue running Hello world application

Hi, I am using STM32MP157D-DK1 board to cross compile my application from host pc.My host PC is installed with ubuntu 20.04. I have setup the build environment in host pc. When i am executing the hello exe in STM32MP board.Please find details below. ...

YRedd.2 by Associate
  • 1684 Views
  • 1 replies
  • 0 kudos

Support for Murata 1YN CYW43439 chipset

Hello everyone,I am trying to integrate the Murata Wi-Fi/BT combo module 1YN in a custom board design based on stm32mp1. The BT part works fine, while the Wi-Fi is not initialized by the system.Apparently, the chipset variant CYW43439 is not supporte...

bimorqt by Associate III
  • 7274 Views
  • 4 replies
  • 0 kudos

How to activate FDCAN in production mode

Dear ST Community,I'm working with fdcan on stm32mp157d-dk1, the fdcan works properly in engineering mode, but i have an issue when in production mode, I found that I have to add the fdcan to the device tree, then I tried to compile the dts generated...

BJlou.1 by Associate II
  • 3282 Views
  • 3 replies
  • 0 kudos