STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I'd like to output the PPS waveform on the STM32MP157D-EV1 board. But it's not outputting.

I found the pin of PG8 on the GPIO pin map on the board. So I connected to PG8 and GND to connect with oscilloscope.In the picture, the blue line is the oscilloscope's GND port.I connected the board and the oscilloscope like the picture above. And I ...

0693W00000aJSdSQAW.png 0693W00000aJSeGQAW.jpg 0693W00000aJSeaQAG.jpg
kKim.1 by Associate II
  • 764 Views
  • 1 replies
  • 0 kudos

Resolved! Can't get GPIOs to work

Hello, Using the stock image I've found I can manipulate the red LED on PA13 by using gpio commands:gpioset gpiochip0 13=0 gpioset gpiochip0 13=1I need to access Pin 38 and Pin 40 on the 40 pin header, which are PI6 and PF11.These are both tied to th...

How to remove "sound" from DTS?

I am trying to use the 40 pin GPIO, namely pin 48 and pin 40 which are PF11 and PI6. PI6 is assigned to sai2. I've disabled sai2. However, the DTB will not compile because there is still a reference to the sai2 pins here:sound:sound{ compatible = ...

DDR addr bus test Error in STM32MP153A

We modified the device tree file corresponding to our development board based on stm32mp157d-ev1.dts.We did not use a PMIC chip, so we added our own power node and modified the default serial port output.This is my device tree file:The following erro...

0693W00000aJJ3vQAG.png 0693W00000aJJ6tQAG.png 0693W00000aJJ8BQAW.png
DG by Associate II
  • 1023 Views
  • 3 replies
  • 0 kudos