2023-03-23 2:03 AM
2023-03-23 2:09 AM
Hi @BJlou.1 ,
Can you try following the Wiki Getting Starting :
Modify, rebuild and reload a firmware - stm32mpu
You have issue while transferring the file to target through Ethernet over USB connexion.
Check the USB OTG connexion.
Olivier
2023-03-23 2:12 AM
actually i tryed an other cable but I have the same problem, I've even tryed to debug another board but I got the samething
2023-03-23 2:15 AM
First ensure you can ping your board @192.168.7.1 from HOST when linux has booted
Share board and OpenSTLinux version + ifconfig output
Olivier
2023-03-23 3:01 AM
the ping command was succefull and i received a rsponse from the board. ( 64 octets de 192.168.7.1 : icmp_seq=27 ttl=64 temps=0.394 ms )
I'm using stm32mp157D-DK1 and stm32mp157F-DK2 boards ( same problem on both boards)
this is the verision of the OpenSTLinux :
ID="openstlinux-weston"
NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro)"
VERSION="2.6-openstlinux-19-12-13 (thud)"
VERSION_ID="2.6-openstlinux-19-12-13"
PRETTY_NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-opens"
2023-03-24 7:45 AM
Hi @BJlou.1 ,
>> VERSION="2.6-openstlinux-19-12-13 (thud)"
Very old version ?!
If you use it with a recent STM32CubeIDE I guess it could be an issue.
I advise you to align the full ecosystem on Version 4.1
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.